3.6 LEDs
The WFI32-IoT on-board LEDs are categorized into three types:
- Power LEDs
 - PKOB4 LEDs
 - LEDs related to the WFI32E01PC module:
 
The following table lists the LEDs that can be turned ON or OFF using the connected GPIO pins.
The WFI32-IoT on-board LEDs are categorized into three types:
The following table lists the LEDs that can be turned ON or OFF using the connected GPIO pins.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.