3.2 Understanding MPLAB Harmony v3 PLIB Generated Code
The following files and folders are generated in the MPLAB Harmony v3 project:
- peripheral: Source and header
files of all the peripherals used in the project are listed inside the
peripheral folder. Usually there will be one
.cand one.hPLIB file per peripheral instance. Some of the peripherals and their files are always added by default in the project, such asgpio,clock,evic. - definitions.h: This file is
similar to the
system_definitions.hfile of MPLAB Harmony v2. It Includes all the header files required for the application. - toolchain_specifics.h: This file has a few macros defined, which are specific to toolchain.
- device.h: This file includes
the headers, which have definitions specific to the selected device, such as
xc.h. - exceptions.c: This file is
same as the
system_exceptions.cfile of MPLAB Harmony v2. It defines the exception handler for the application. - initialization.c: This file is
same as the
system_init.cfile of MPLAB Harmony v2. It initializes all the MPLAB Harmony modules used in the application. - interrupts.c: This file is
same as the
system_interrupt.cfile of MPLAB Harmony v2. It contains definitions of all the interrupt service routines used in the application. - stdio/xc32_monitor.c: A new
feature is added in MPLAB Harmony v3 to support the
printfandscanffunctions of the standard C library. When the STDIO module (listed in Tools in the Device Resources window) is used, the function definitions inside this file get updated by the MCC to make theprintfandscanffunctions work. - main.c: This file is same as
in MPLAB Harmony v2. However, in MPLAB Harmony v2 it is recommended to develop the
application in
app.c. In a MPLAB Harmony v3 PLIB only project, it is recommended to do it inmain.c. MPLAB Harmony v3 driver-based applications are still recommended to be developed inapp.c.