2 MPLAB Code Configurator GUI
The MPLAB Code Configurator (MCC) is a GUI-based tool that provides an easy way to enable, configure and generate codes for various MPLAB Harmony modules. In MPLAB X IDE, the MCC plugin is installed by default.
To update the MCC plugin to the new version for MPLAB Harmony v3, follow these steps:
- Open MPLAB X IDE.
- Select Tools > Plugins, and then click on the Installed tab. The MCC can be found in the list of installed plugins.
- In the Installed tab, if an update is available, an Update button will appear. Click on the Update button to install the latest version of the MCC plugin.
- Select Restart Now to apply the updates.
In MPLAB Harmony v2, all modules are arranged in a tree structure, and can be configured by expanding the '+' sign. However, in MPLAB Harmony v3, multiple windows are available to make the configuration easier and intuitive. The following figure shows the MPLAB Code Configurator window.