3.6 Comparison Between MPLAB Harmony v2 and MPLAB Harmony v3 PLIB Examples
If application development steps in MPLAB Harmony v2 and MPLAB Harmony v3 are compared for the given example, the following differences can be noticed:
- MPLAB Harmony v3 has one MCC configuration step 2.2 extra
- MPLAB Harmony v3 has one coding step 4.1 less
- MPLAB Harmony v3 has application logic step 4.2 simplified
The previous example is of a very simple application. As the application complexity increases, the differences will become more evident and it becomes much simpler and user friendly to develop applications using MPLAB Harmony v3 PLIBs as compared to MPLAB Harmony v2.