42.6.2.4.4 Start Event Action
The start action can be selected in the Event Control register (EVCTRL.EVACT0 = 0x3, START) and can start the counting operation when previously stopped. The event has no effect if the counter is already counting. When the module is enabled, the counter operation starts when the event is received or when a re-trigger software command is applied.
Note: When a start event action is configured
in the Event Action bits in the Event Control register (EVCTRL.EVACT0 = 0x3, START),
enabling the counter will not start the counter. The counter starts on the next incoming
event, but it will not restart on subsequent events.