37.11 ADC Sampling Requirements
The analog input model of the 12-bit ADC is illustrated in the following figure. The total acquisition time for the analog-to-digital conversion is a function of the internal circuit settling time and the holding capacitor charge time.
For the ADC core to meet its specified accuracy, the charge holding capacitor (CSamp) must be allowed to fully charge to the voltage level on the analog input pin. The analog output source impedance (RSRC), the interconnect impedance (RIC) and the internal sampling switch (RIN_ADC) impedance combine to directly affect the time required to charge the CSamp. The combined impedance of the analog sources must, therefore, be small enough to fully charge (to within one-fourth LSB of the desired voltage) the holding capacitor within the selected sample time. The internal holding capacitor is in the discharged state prior to each sample operation.
One TAD7 time period must be allowed between conversions for the acquisition time. See Electrical Characteristics from Related Links.
- CPIN = 4pF (Input capacitance)
- RIN_ADC = 200Ω (Sampling switch resistance)
- RSRC = Source resistance
- ILEAKAGE = Leakage current at the pin due to various junctions
- VT = Threshold voltage
- RIC = 60Ω for dedicated ADC and 45Ω for shared ADC
- CSamp = 5 pF (Sample/hold capacitance)
- R_PAD = 510Ω, including ESD + Switch resistance
- C_int = 0 pF for dedicated and 9.2 pF for shared ADC (sum of switches connected to internal net and the routing capacitance)