42.7.5.4.3 General Call
The general call is performed in order to change the address of the client.
If a GENERAL CALL is detected, GACC is set.
After the detection of general call, decode the commands that follow.
In case of a WRITE command, decode the programming sequence and program a new SADR if the programming sequence matches.
The following figure describes the general call access.
Note: This method enables the user to create a
personal programming sequence by choosing the programming bytes and their number. The
programming sequence has to be provided to the Host.