12.1.3.1 PFM Erase Sequence
The sequence of events for erasing a block of internal program memory is:
- Set NVMADR to an address within the intended sector.
- Set the NVMEN bit to enable NVM
- Perform the unlock sequence as described the NVM Unlock Sequence section
- Set the SECER bit
If the PFM address is write-protected, the SECER bit will be cleared and the erase operation will not take place, NVMERR is signaled in this scenario.
The operation erases the sector indicated by masking the LSbs of the current NVMADR.
While erasing PFM, CPU operation is suspended and it resumes when the operation is complete. Upon completion the SECER bit is cleared in hardware, the NVMIF is set and an interrupt will occur if the NVMIE bit is also set.
The holding register data are not affected by erase operations and NVMEN will remain unchanged.
Erasing a Program Flash Memory block
; This sample sector erase routine assumes that the target address
; specified by CODE_ADDR_UPPER and CODE_ADDR_HIGH contain a value within
; the PFM address range of the device.
MOVLW CODE_ADDR_UPPER ; load NVMADR with the base
MOVWF NVMADRU ; address of the memory block
MOVLW CODE_ADDR_HIGH
MOVWF NVMADRH
ERASE_BLOCK:
BSF NVMCON0, NVMEN ; enable Program Flash Memory
BCF INTCON, GIE ; disable interrupts
Required MOVLW CCh ; first unlock byte for erase
Sequence MOVWF NVMCON2 ; write CCh
MOVLW 33h ; second unlock byte for erase
MOVWF NVMCON2 ; write 33h
BSF NVMCON1, SECER ; start erase (CPU stalls)
BSF INTCON, GIE ; re-enable interrupts
BCF NVMCON0, NVMEN ; disable writes to memory
- If a write or erase operation is terminated by an unexpected event, NVMERR bit will be set which the user can check to decide whether a rewrite of the location(s) is needed.
- NVMERR is set if SECER is written
to ‘
1’ while NVMADR points to a write-protected address. - NVMERR is set if SECER is written
to ‘
1’ while NVMADR points to an invalid address location ( Refer to the device memory map and NVM Organization Table).