6.2.4 Import Other Embedded Projects
MPLAB X IDE can create a project from selected, other embedded projects. There are two methods to import these projects.
Import Project Option
- Select .
- Select from a list of available embedded projects.
- Continue to create an MPLAB X IDE project.
New Project Option
- Select .
- Click on Other Embedded under Categories and select from a list of available embedded projects.
- Continue to create an MPLAB X IDE project.
This feature imports your existing files into an MPLAB X IDE project.
IAR Embedded Workbench®
The device names used in an IAR project may be slightly different from the device names used in an MPLAB X IDE project. Please verify that the suggested device is correct.
For an MPLAB XC C compiler selected as the toolchain, the following settings in the IAR project are imported into the resulting MPLAB X IDE:
- Project files
- Include directories
- Defined symbols (called "Preprocessor macros" in the MPLAB X IDE project)
You must configure all other compiler settings manually. Consult the MPLAB XC8 C Compiler User’s Guide for AVR MCU (DS-50002750) or MPLAB XC32 C/C++ Compiler User's Guide for PIC32C/SAM MCUs (DS-50002895) for more information.
Additional Information
For information on how to work with MPLAB X IDE, see:
For information on available compilers, see: