6.3 Project Types
The New Project wizard supports the following project types:
- Microchip Embedded
- Application Project(s) - Several types are discussed in the following sections.
- Prebuilt (Hex, Loadable Image) Project - This type of project is imported. See Import Prebuilt Projects.
- User Makefile Project - This type of project is discussed in a following section.
- Libraray Project - This type of project is discussed in a following section.
- Other Embedded - These types of projects are imported. See Import Other Embedded Projects.
- Generic - The “Group of Projects” type is discussed in a following section.