5.1.1 Same Board Communication
(Ask a Question)To setup same board communication, perform the following steps:
- Connect the AD9371 with the FMC Connector of the PolarFire FPGA Evaluation kit.
- Connect the SMA antenna at the transmitter and other SMA antenna at the receiver part as shown in the Figure 7-2.
- Ensure that the jumper setting are as per the Table 5-1 and power up the board.