5.1.2 Two Boards Communication

To setup two boards communication, perform the following steps:

  1. Connect the AD9371 with the FMC Connector of the PolarFire FPGA Evaluation kit and follow the same for the other board.
  2. Connect the SMA antenna at the Transmitter of board 1 and connect the other antenna at the receiver of the board 2 as shown in Figure 7-1.
  3. Ensure that the jumper settings are as per the Table 5-1, and the board is powered up and the same must be done with the second board.