5.1 Setting Up the Hardware
(Ask a Question)After generating the bitstream, the PolarFire device is programmed on Evaluation kit by performing the following steps:
- Ensure that the jumper settings on the board are same as listed in the following table.
Table 5-1. Jumper Settings Jumper Description J18, J19, J20, J21, J22 Close pin 2 and 3 for programming the PolarFire FPGA through FTDI J28 Close pin 1 and 2 for programming through the on-board FlashPro5 J26 Close pin 1 and 2 for programming through the FTDI SPI J27 Close pin 1 and 2 for programming through the FTDI SPI J4 Close pin 1 and 2 for manual power switching using SW3 J12 Close pin 3 and 4 for 2.5 V J23 Remain open SW11 Switch 1 and 2. Selects Tx and Rx LO (Local Oscillator) frequency in AD9371. For more information, see Changing the Tx and Rx frequency section. SW5 Reset switch - Connect the power supply cable to the J9 connector on the board.
- Connect the USB cable from the host PC to the J5 (FTDI port) on the board.
- Power on the board using the SW3 slide switch.
- For external loop back demo, connect TX1 to RX1 using the 1 SMA to SMA cables.
The following figure shows the board setup for the mentioned jumper settings.
When the board is powered up, power supply LEDs DS3 to DS14 is switched on. For more information about LEDs on the PolarFire FPGA Evaluation Kit, see UG0747: PolarFire FPGA Evaluation Kit User Guide.