3.4.14.1 DFK Database and Manufacturing Keys
U-HSM prepares DFK DB for M-HSM, which contains information about DFK and manufacturing keys. This database is a file with the name following this pattern:
DFK-<U_UUID>.DFKDB, where U_UUID is the UUID of the U-HSM (this is not the M-HSM UUID).
For example, DFK-00000000000000000000000000000001.DFKDB.
M-HSM imports device information using the following command:
M-HSMImportDeviceData.exe <DFKDB_file>
This step imports DFKDB and device-type specific manufacturing keys. If any of those manufacturing keys have already been imported, the utility ignores them.
For each imported manufacturing key, a new file is created in the key folder of the
Security World. The file has the following format:
key_simple_g4mf-klk-<device_key_uuid>.
For example,
key_simple_g4mf-klk-1000000000000000000000000000000000000005.