32.4.2.6 Sequential Logic
Each LUT pair can be connected to the internal sequential logic, which can be configured to operate as a D flip-flop, JK flip-flop, gated D latch, or RS latch by configuring the Sequential Selection bits in the corresponding Sequential Control (SEQCTRL) register. Before using sequential logic, the GCLK_CCL clock must be enabled, and, if required, each LUT filter or edge detector should also be enabled.
Gated D Flip-Flop (DFF)
When D flip-flop (DFF) mode is selected, the D input is driven by the even LUT output (LUT0 or LUT2), and the G input is driven by the odd LUT output (LUT1 or LUT3), as illustrated in the figure below.
The flip-flop output (OUT) is updated on the rising edge of the GCLK_CCL, as shown in the table below.
| R | G | D | OUT |
|---|---|---|---|
| 1 | X | X | Clear |
| 0 | 1 | 1 | Set |
| 0 | Clear | ||
| 0 | X | Hold state (no change) |
JK Flip-Flop (JK)
When this configuration is selected, the J input is driven by the even LUT output (LUT0 or LUT2), and the K input is driven by the odd LUT output (LUT1 or LUT3), as illustrated in the figure below.
The flip-flop output (OUT) is updated on the rising edge of GCLK_CCL, as shown in the table below.
| R | J | K | OUT |
|---|---|---|---|
| 1 | X | X | Clear |
| 0 | 0 | 0 | Hold state (no change) |
| 0 | 0 | 1 | Clear |
| 0 | 1 | 0 | Set |
| 0 | 1 | 1 | Toggle |
Gated D Latch (DLATCH)
When DLATCH is selected, the D input is driven by the even LUT output (LUT0 or LUT2), and the G input is driven by the odd LUT output (LUT1 or LUT3), as illustrated in the figure below.
The latch output (OUT) is updated as shown in the table below.
| G | D | OUT |
|---|---|---|
| 0 | X | Hold state (no change) |
| 1 | 0 | Clear |
| 1 | 1 | Set |
RS Latch (RS)
When this configuration is selected, the S input is driven by the even LUT output (LUT0 or LUT2), and the R input is driven by the odd LUT output (LUT1 or LUT3), as illustrated in the figure below.
The latch output (OUT) is updated as shown in the table below.
| S | R | OUT |
|---|---|---|
| 0 | 0 | Hold state (no change) |
| 0 | 1 | Clear |
| 1 | 0 | Set |
| 1 | 1 | Forbidden state |