5.1.3.5 Data Capture for Balanced and Unbalanced Loads

Data capture will happen in snapshots, and several snapshots will be captured for each one of the classes:

  • Unbalanced
  • Normal Operation

Data capture steps will be repeated on every snapshot.

The motor will be in normal operation when using a balanced load disc.

Figure 5-19. Motor with a Balanced Load Disc on the Rotor
???

And in unbalanced operation when using an unbalanced load disc.

Figure 5-20. Motor with an Unbalanced Load Disc on the Rotor
???

Load discs can be printed using the STL files provided in the stl-files folder from the companion material.

Note: Delete the cursors A and B before capturing the next snapshot.
Figure 5-21. MPLAB® Data Visualizer Time Plot Cursor Location
???