1.1 Overlay Selection
On many devices, all CLCs share the same set of register addresses; this is known as an overlay. In these instances, only one CLC may be accessed at one time. The CLC to be configured is selected first by using the CLCSELECT register. The value of CLCSELECT is one less than the selected CLC. For example, CLCSELECT=0 selects CLC1.