A slider control can now be added to the dashboard.
Todo:
Select the Edit checkbox
Open the Elements tab
Drag a Slider element onto
the dashboard
A slider control needs to have some configuration
parameters.
Todo: Select the slider element and set
its properties:
Maximum = 500
Minimum = 100
A segment display control can now be added to the dashboard.
Todo:
Select the Edit checkbox
Open the Elements tab
Drag a Segment Display
element onto the dashboard
A segment display control needs to have some
configuration parameters.
Todo: Select the segment display element
and set its properties:
Segment Count = 3
The slider control can now be used as a source which can be connected to any
relevant sink in Data Visualizer. The segment display can similarly be used as a sink to
connect any relevant source to.
The Code Profiling data polling interface provides
both a source of data and a sink of data. The slider can now be connected to the sink
and the segment display to the source.
Todo:
Deselect the Edit
checkbox
Select the Show Endpoints
checkbox
Connect sources to sinks by
dragging each source plug and drop it on a
sink
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.