3.3.2.1 How to Add Project Libraries

Tip:

Ensure you have library projects in the current solution.

Steps to add libraries to an application project:
  1. Right click on the project, or ‘Libraries’ node in the project, to invoke the 'Add Library' wizard.
  2. Select the ‘Project Libraries’ tab; all the library projects in the current solution will be listed here.
  3. Select the library project which you would like to add.
  4. Click OK to complete.
Figure 3-24. Add Library Context Menu
Figure 3-25. Add Project Library
Figure 3-26. View of a Project After Adding Libraries

Also, see that the library was added as project dependency from Project → Build Dependencies → Project Dependencies.

Figure 3-27. View of Project Dependencies View After Adding Project Libraries