3.3.2.2 How to Add Toolchain Libraries

  1. Right click on the project, or ‘Libraries’ node in the project, to invoke the 'Add Library' wizard.
  2. Select the ‘Toolchain Libraries’ tab.
  3. The list of available toolchain libraries will be listed here.
  4. Select the libraries which you would like to add.
  5. Click OK to complete.
Figure 3-28. Add Library Context Menu
Figure 3-29. Add Library Dialog
Figure 3-30. View of a Solution With XC8 Project After Adding Libraries

You can also see the new library added in the Toolchain Linker Settings from the Project → Properties → Toolchain tab.

Figure 3-31. View of Linker Option After Adding Libraries