29.4.4 GPNVM Bit

The Flash memory features 9 General Purpose Non Volatile Memory bits.

GPNVM bits do not interfere with the embedded Flash memory plane. For more details, refer to the section “Memories”.

The ‘Set GPNVM Bit’ sequence is the following:

  1. Execute the ‘Set GPNVM Bit’ command by writing EEFC_FCR.FCMD with the SGPB command and EEFC_FCR.FARG with the number of GPNVM bits to be set.
  2. When the GPNVM bit is set, the bit EEFC_FSR.FRDY rises. If an interrupt was enabled by setting the bit EEFC_FMR.FRDY, the interrupt line of the interrupt controller is activated.
  3. The result of the SGPB command can be checked by running a ‘Get GPNVM Bit’ (GGPB) command.
    Note: The value of the FARG argument passed together with SGPB command must not exceed the higher GPNVM index available in the product. Flash data content is not altered if FARG exceeds the limit. Command Error is detected only if FARG is greater than 8.

Two errors can be detected in EEFC_FSR after a programming sequence:

  • Command error: a wrong keyword was written in EEFC_FCR.
  • Flash error: at the end of the programming, the EraseVerify or WriteVerify test of the Flash memory has failed.

It is possible to clear GPNVM bits previously set. The ‘Clear GPNVM Bit’ sequence is the following:

  1. Execute the ‘Clear GPNVM Bit’ command by writing EEFC_FCR.FCMD with the CGPB command and EEFC_FCR.FARG with the number of GPNVM bits to be cleared.
  2. When the clear completes, the bit EEFC_FSR.FRDY rises. If an interrupt was enabled by setting the bit EEFC_FMR.FRDY, the interrupt line of the interrupt controller is activated.
    Note: The value of the FARG argument passed together with the CGPB command must not exceed the highest GPNVM index available in the product. Flash data content is not altered if FARG exceeds the limit. A command error is detected only if FARG is greater than 8.
Important: GPNVM bits are set and cleared on a bit-by-bit basis and extreme caution must be used during the configuration sequence to avoid triggering undesired operations. As an example, if the bit-by-bit setting/clearing of GPNVM[4:2] results in the sequence '110' at any time during configuration, the EFL mode is set to "HW Erase function disabled - EFL bits are read-only". This mode permanently disables the Hardware Erase signal, the Flash can no longer be erased, and the operation is irreversible.

For a full description of GPNVM bit settings and functions, see the table "GPNVM Bits Overview" in the section "ROM Code and Boot Strategies”.

Two errors can be detected in EEFC_FSR after a programming sequence:

  • Command error: a wrong keyword was written in EEFC_FCR.
  • Flash error: at the end of the programming, the EraseVerify or WriteVerify test of the Flash memory has failed.

The status of the GPNVM bits can be returned by the SEFC. The sequence is the following:

  1. Execute the ‘Get GPNVM Bit’ command by writing EEFC_FCR.FCMD with the GGPB command. Field EEFC_FCR.FARG is meaningless.
  2. GPNVM bits can be read by the software application in EEFC_FRR. The first word read corresponds to the first 32 GPNVM bits; the following reads provide the next 32 GPNVM bits as long as it is meaningful. Extra reads to EEFC_FRR return 0.

For example, if the third bit of the first word read in EEFC_FRR is set, the third GPNVM bit is active.

One error can be detected in EEFC_FSR after a programming sequence:

  • Command error: a wrong keyword was written in EEFC_FCR.
    Note: Access to the Flash in read is permitted when a ‘Set GPNVM Bit’, ‘Clear GPNVM Bit’ or ‘Get GPNVM Bit’ command is executed, but the access is stalled until the command is completed.