1.1.6.4.9 DRV_SDMMC_GeometryGet Function
C
SYS_MEDIA_GEOMETRY* DRV_SDMMC_GeometryGet ( const DRV_HANDLE handle );
Summary
Returns the geometry of the device.
Description
This API gives the following geometrical details of the SD Card.
- Media Property
- Number of Read/Write/Erase regions in the SD Card
- Number of Blocks and their size in each region of the device
Precondition
The DRV_SDMMC_Initialize routine must have been called for the specified SDMMC driver instance.
The DRV_SDMMC_Open routine must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open function |
Returns
SYS_MEDIA_GEOMETRY - Pointer to structure which holds the media geometry information.
Example
SYS_MEDIA_GEOMETRY* SDMMCGeometry; uint32_t readBlockSize, writeBlockSize, eraseBlockSize; uint32_t nReadBlocks, nReadRegions, totalSize; SDMMCGeometry = DRV_SDMMC_GeometryGet(SDMMCOpenHandle1); readBlockSize = SDMMCGeometry->geometryTable->blockSize; nReadBlocks = SDMMCGeometry->geometryTable->numBlocks; nReadRegions = SDMMCGeometry->numReadRegions; writeBlockSize = (SDMMCGeometry->geometryTable +1)->blockSize; eraseBlockSize = (SDMMCGeometry->geometryTable +2)->blockSize; totalSize = readBlockSize * nReadBlocks * nReadRegions;
Remarks
Refer sys_media.h for definition of SYS_MEDIA_GEOMETRY.