1.1.6.4.4 DRV_SDMMC_Open Function
C
DRV_HANDLE DRV_SDMMC_Open (
const SYS_MODULE_INDEX drvIndex,
const DRV_IO_INTENT intent
);Summary
Opens the specified SD Card driver instance and returns a handle to it.
Description
This routine opens the specified SDMMC driver instance and provides a handle that must be provided to all other client-level operations to identify the caller and the instance of the driver.
Precondition
Function DRV_SDMMC_Initialize must have been called before calling this function.
Parameters
| Param | Description |
|---|---|
| drvIndex | Identifier for the object instance to be opened |
| intent | Zero or more of the values from the enumeration DRV_IO_INTENT "ORed" together to indicate the intended use of the driver |
Returns
If successful, the routine returns a valid open-instance handle (a number identifying both the caller and the module instance).
If an error occurs, the return value is DRV_HANDLE_INVALID.
Example
DRV_HANDLE handle;
handle = DRV_SDMMC_Open (DRV_SDMMC_INDEX_0, DRV_IO_INTENT_EXCLUSIVE);
if (handle == DRV_HANDLE_INVALID)
{
// Unable to open the driver
}Remarks
The handle returned is valid until the DRV_SDMMC_Close routine is called.