1.1.6.4.11 DRV_SDMMC_IsAttached Function
C
bool DRV_SDMMC_IsAttached ( const DRV_HANDLE handle );
Summary
Returns the physical attach status of the SD Card.
Description
This function returns the physical attach status of the SD Card.
Precondition
The DRV_SDMMC_Initialize routine must have been called for the specified SDMMC driver instance. The DRV_SDMMC_Open routine must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open function |
Returns
Returns false if the handle is invalid otherwise returns the attach status of the SD Card. Returns true if the SD Card is attached and initialized by the SDMMC driver otherwise returns false.
Example
// drvSDMMCHandle is the handle returned // by the DRV_SDMMC_Open function. bool isSDMMCAttached; isSDMMCAttached = DRV_SDMMC_isAttached(drvSDMMCHandle);
Remarks
None.