1.3.1.4.3 EMU_EEPROM_FormatMemory Function
C
bool EMU_EEPROM_FormatMemory(void)Summary
Erases the entire emulated EEPROM memory space.
Description
Erases the entire emulated EEPROM memory space and formats it.
Precondition
Function EMU_EEPROM_Initialize should have been called before calling this function.
Parameters
None
Returns
True - Memory is formatted successfully
False - Error during formatting
Example
if (EMU_EEPROM_Status() == SYS_STATUS_UNINITIALIZED)
{
//Format the EEPROM Emulation memory if the initialization failed
EMU_EEPROM_FormatMemory();
}Remarks
None