1.2.1.21 SYS_MODULE_TASKS_ROUTINE Typedef
C
typedef void (* SYS_MODULE_TASKS_ROUTINE) ( SYS_MODULE_OBJ object );
Summary
Pointer to a routine that performs the tasks necessary to maintain a state machine in a module system module (driver, library, or system-maintained application).
Description
This data type is a pointer to a routine that performs the tasks necessary to maintain a state machine in a module system module (driver, library, or system-maintained application).
Precondition
The low-level board initialization must have (and will be) completed and the module's initialization routine will have been called before the system will call the deinitialization routine for any modules.
Parameters
| Param | Description |
|---|---|
| object | Handle to the module instance |
Returns
None.
Example
None.
Remarks
If the module is interrupt driven, the system will call this routine from an interrupt context.