1.1.9.4.14 DRV_USART_ReadAbort Function
C
bool DRV_USART_ReadAbort(const DRV_HANDLE handle)Summary
Aborts an on-going read request
Description
This function aborts an on-going read transfer. No callback is given for the on-going request being aborted. When USART is configured for non-dma transfers, application may call the DRV_USART_BufferCompletedBytesGet() API (before calling the DRV_USART_ReadAbort API)to find out how many bytes have been received for the on-going read request.
Precondition
DRV_USART_Open must have been called to obtain a valid opened device handle.
Parameters
| Param | Description |
|---|---|
| handle | Handle of the communication channel as return by the DRV_USART_Open function. |
Returns
true - operation was successful
false - error in running the API
Example
// myUSARTHandle is the handle returned // by the DRV_USART_Open function. // For non-DMA based transfers DRV_USART_BufferCompletedBytesGet() can be // called to find out the number of bytes received before aborting the // request. uint32_t processedBytes; processedBytes= DRV_USART_BufferCompletedBytesGet(bufferHandle); DRV_USART_ReadAbort(myUSARTHandle);
Remarks
This function is thread safe in a RTOS application. Calling this function does not have any impact on the read/write requests that may be pending in the transfer queue. To purge the read/write request queues call the DRV_USART_ReadQueuePurge() and DRV_USART_WriteQueuePurge() APIs.