1.1.9.4.19 DRV_USART_BUFFER_EVENT Enum
C
typedef enum
{
/* The buffer is pending to be serviced */
DRV_USART_BUFFER_EVENT_PENDING = 0,
/* All data from or to the buffer was transferred successfully. */
DRV_USART_BUFFER_EVENT_COMPLETE = 1,
/* Transfer Handle given is expired. It means transfer
is completed but with or without error is not known. */
DRV_USART_BUFFER_EVENT_HANDLE_EXPIRED = 2,
/* There was an error while processing the buffer transfer request. */
DRV_USART_BUFFER_EVENT_ERROR = -1,
/* Transfer Handle given is invalid */
DRV_USART_BUFFER_EVENT_HANDLE_INVALID = -2
} DRV_USART_BUFFER_EVENT;
Summary
Identifies the possible events that can result from a buffer add request.
Description
This enumeration identifies the possible events that can result from a buffer add request caused by the client calling either the DRV_USART_ReadBufferAdd or DRV_USART_WriteBufferAdd functions.
Remarks
One of these values is passed in the "event" parameter of the event handling callback function that the client registered with the driver by calling the DRV_USART_BufferEventHandlerSet function when a buffer transfer request is completed.