1.1.9.4.5 DRV_SPI_TransferSetup Function

1.1.9.4.5 C

bool DRV_SPI_TransferSetup ( DRV_HANDLE handle, DRV_SPI_TRANSFER_SETUP * setup )

1.1.9.4.5 Summary

Sets the dynamic configuration of the driver including Chip Select pin. Application must call this API and configure the transfer parameters before starting any data transfers.

1.1.9.4.5 Description

This function is used to update any of the DRV_SPI_TRANSFER_SETUP parameters for the selected client of the driver dynamically. For single client scenario, if GPIO has to be used for Chip Select, then calling this API with appropriate GPIO pin information becomes mandatory. For multi-client scenario where different clients need different setup, such as baud rate, clock settings, Chip Select, etc, then also calling this API is mandatory.

Note that all the elements of setup structure must be filled appropriately before using this API.

1.1.9.4.5 Preconditions

DRV_SPI_Open must have been called to obtain a valid opened device handle.

1.1.9.4.5 Parameters

ParametersDescription
handleA valid open-instance handle, returned from the driver's open routine
*setupA structure containing the new configuration settings

1.1.9.4.5 Returns

None.

1.1.9.4.5 Example

// mySPIHandle is the handle returned by the DRV_SPI_Open function.
DRV_SPI_TRANSFER_SETUP setup;

setup.baudRateInHz = 10000000;
setup.clockPhase = DRV_SPI_CLOCK_PHASE_TRAILING_EDGE;
setup.clockPolarity = DRV_SPI_CLOCK_POLARITY_IDLE_LOW;
setup.dataBits = DRV_SPI_DATA_BITS_16;
setup.chipSelect = SYS_PORT_PIN_PC5;
setup.csPolarity = DRV_SPI_CS_POLARITY_ACTIVE_LOW;

DRV_SPI_TransferSetup ( mySPIHandle, &setup );

1.1.9.4.5 Remarks

None.