1.1.9.4.2 DRV_SPI_Status Function
1.1.9.4.2 C
SYS_STATUS DRV_SPI_Status( SYS_MODULE_OBJ object )1.1.9.4.2 Summary
Gets the current status of the SPI driver module.
1.1.9.4.2 Description
This routine provides the current status of the SPI driver module.
1.1.9.4.2 Precondition
Function DRV_SPI_Initialize should have been called before calling this function.
1.1.9.4.2 Parameters
| Parameters | Description |
|---|---|
| object | Driver object handle, returned from the DRV_SPI_Initialize routine |
1.1.9.4.2 Returns
SYS_STATUS_READY - Initialization have succeeded and the SPI is ready for additional operations.
SYS_STATUS_DEINITIALIZED - Indicates that the driver has been deinitialized.
1.1.9.4.2 Example
SYS_MODULE_OBJ object; // Returned from DRV_SPI_Initialize
SYS_STATUS spiStatus;
spiStatus = DRV_SPI_Status(object);
if (spiStatus == SYS_STATUS_READY)
{
// This means now the driver can be opened using the
// DRV_SPI_Open() function.
}1.1.9.4.2 Remarks
A driver can be opened only when its status is SYS_STATUS_READY.