1.1.6.4.3 DRV_SDMMC_Tasks Function

C

void DRV_SDMMC_Tasks ( SYS_MODULE_OBJ object );

Summary

Maintains the driver's state machine.

Description

This routine is used to maintain the driver's internal state machine.

Precondition

The DRV_SDMMC_Initialize routine must have been called for the specified SDMMC driver instance.

Parameters

ParametersDescription
objectObject handle for the specified driver instance (returned from DRV_SDMMC_Initialize)

Returns

None.

Example

SYS_MODULE_OBJ object; // Returned from DRV_SDMMC_Initialize

while (true)
{
    DRV_SDMMC_Tasks (object);

    // Do other tasks
}

Remarks

This routine is normally not called directly by an application. It is called by the system's Tasks routine (SYS_Tasks).