1.1.6.4.15 DRV_SDMMC_Async_SDIO_ExtBytesWrite Function

C

void DRV_SDMMC_Async_SDIO_ExtBytesWrite (
    const DRV_HANDLE handle,
    DRV_SDMMC_COMMAND_HANDLE* commandHandle,
    uint8_t fn,
    uint32_t regAddr,
    void* wrData,
    uint32_t nBytes,
    bool isAddrInc
)

Summary

Writes multiple bytes of data starting at the specified regAddr of the SDIO card.

Description

This function schedules a non-blocking write operation for writing multiple bytes of data (using CMD53) to the given I/O function in the SDIO card. The API allows the application to specify whether to increment or not the I/O address after each byte is written. The number of bytes to write must be between 1 and 511. The function returns with a valid buffer handle in the commandHandle argument if the write request was scheduled successfully. The function adds the request to the hardware instance queue and returns immediately. While the request is in the queue, the application buffer is owned by the driver and should not be modified. The function returns DRV_SDMMC_COMMAND_HANDLE_INVALID in the commandHandle argument under the following circumstances:

  • if the driver handle is invalid

  • if the wrData pointer is NULL or nBytes is 0

  • if the nBytes is not between 1 and 511

  • if the media is not in attached state

  • if a buffer object could not be allocated to the request

If the requesting client registered an event callback with the driver, the driver will issue a DRV_SDMMC_EVENT_COMMAND_COMPLETE event if the buffer was processed successfully or DRV_SDMMC_EVENT_COMMAND_ERROR event if the buffer was not processed successfully.

Precondition

The DRV_SDMMC_Initialize routine must have been called for the specified SDMMC driver instance.

DRV_SDMMC_Open routine must have been called to obtain a valid opened device handle.

Parameters

ParametersDescription
handleA valid open-instance handle, returned from the driver's open function.
commandHandlePointer to the buffer handle returned by this API.
fnThe function number within the SDIO card to write to.
regAddrStart address of I/O register to write the data to.
wrDataPointer to the buffer containing the data to be written.
nBytesNumber of bytes of data to be written. Its value must be from 1 to 511.
isAddrIncTrue - increment the I/O register address after each write.

Returns

The buffer handle is returned in the commandHandle argument. It will be DRV_SDMMC_COMMAND_HANDLE_INVALID if the request was not successful.

Example

uint8_t CACHE_ALIGN myBuffer[16];

// address should be block aligned.
uint32_t reg_addr = 0x1000;
uint32_t nBytes = 16;
DRV_SDMMC_COMMAND_HANDLE commandHandle;

// Event is received when the buffer is processed.

void APP_SDMMCEventHandler(
    DRV_SDMMC_EVENT event,
    DRV_SDMMC_COMMAND_HANDLE commandHandle,
    uintptr_t contextHandle
)
{
    switch(event)
    {
        case DRV_SDMMC_EVENT_COMMAND_COMPLETE:
        {
            // This means the data was transferred successfully
            break;
        }

        case DRV_SDMMC_EVENT_COMMAND_ERROR:
        {
            // Error handling here
            break;
        }

        default:
        {
            break;
        }
    }
}

// mySDMMCHandle is the handle returned
// by the DRV_SDMMC_Open function.

// Client registers an event handler with driver

DRV_SDMMC_EventHandlerSet(mySDMMCHandle, APP_SDMMCEventHandler, (uintptr_t)NULL);

DRV_SDMMC_Async_SDIO_ExtBytesWrite (
    mySDMMCHandle,
    &commandHandle,
    1,
    reg_addr,
    myBuffer,
    nBytes,
    true
);

if(commandHandle == DRV_SDMMC_COMMAND_HANDLE_INVALID)
{
    // Error handling here
}

Remarks

None.