1.1.6.4.2 DRV_SDMMC_Status Function
C
SYS_STATUS DRV_SDMMC_Status ( SYS_MODULE_OBJ object );
Summary
Provides the current status of the SD card driver module.
Description
This routine provides the current status of the SD card driver module.
Precondition
Function DRV_SDMMC_Initialize must have been called before calling this function.
Parameters
| Parameters | Description |
|---|---|
| object | Driver object handle, returned from the DRV_SDMMC_Initialize routine |
Returns
SYS_STATUS_READY - Indicates that the driver is busy with a previous system level operation and cannot start another. Any value greater than SYS_STATUS_READY is also a normal running state in which the driver is ready to accept new operations.
SYS_STATUS_UNINITIALIZED - Driver is not initialized.
Example
SYS_MODULE_OBJ object; // Returned from DRV_SDMMC_Initialize
SYS_STATUS status;
status = DRV_SDMMC_Status(object);
if (status == SYS_STATUS_READY)
{
// Driver is initialized and ready to accept requests
}Remarks
None.