DRV_SST39_Initialize Function
C
SYS_MODULE_OBJ DRV_SST39_Initialize
(
const SYS_MODULE_INDEX drvIndex,
const SYS_MODULE_INIT *const init
)Summary
Initializes the SST39 Driver.
Description
This routine initializes the SST39 driver making it ready for client to use.
Precondition
None.
Parameters
| Parameters | Description |
|---|---|
| drvIndex | Identifier for the instance to be initialized |
| init | Pointer to a data structure containing any data necessary to initialize the driver |
Returns
If successful, returns a valid handle to a driver instance object. Otherwise, it returns SYS_MODULE_OBJ_INVALID.
Example
// This code snippet shows an example of initializing the SST39 Driver
// with SST39 Parallel flash device attached.
SYS_MODULE_OBJ objectHandle;
const DRV_SST39_PLIB_INTERFACE drvSST39PlibAPI = {
.write = (DRV_SST39_PLIB_WRITE)HEMC_Write8,
.read = (DRV_SST39_PLIB_READ)HEMC_Read8,
.eccDisable = (DRV_SST39_PLIB_ECC_DISABLE)HEMC_DisableECC,
.eccEnable = (DRV_SST39_PLIB_ECC_ENABLE)HEMC_EnableECC,
};
const DRV_SST39_INIT drvSST39InitData =
{
.sst39Plib = &drvSST39PlibAPI,
};
objectHandle = DRV_SST39_Initialize((SYS_MODULE_INDEX)DRV_SST39_INDEX, (SYS_MODULE_INIT *)&drvSST39InitData);
if (SYS_MODULE_OBJ_INVALID == objectHandle)
{
printf("Initialization Error");
}Remarks
This routine must be called before any other SST39 driver routine is called.
This routine should only be called once during system initialization.