DRV_SST39_ReadProductId Function
C
bool DRV_SST39_ReadProductId( const DRV_HANDLE handle, uint8_t* manufacturer, uint8_t* device )Summary
Reads Manufacturer and Device ID of the SST39 device.
Description
This function schedules a blocking operation for reading the Manufacturer and Device ID.
Preconditions
The DRV_SST39_Open() routine must have been called for the specified SST39 driver instance.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| manufacturer | Pointer to 8-bit variable that will be updated with read manufacturer value |
| device | Pointer to 8-bit variable that will be updated with read device value |
Returns
True - If the read is successfully completed.
False - If command fails.
Example
DRV_HANDLE handle; uint8_t manufacturer = 0; uint8_t device = 0; if(DRV_SST39_ReadProductId(appData.handle, &manufacturer, &device) == false) { printf("Error handling here"); }
Remarks
None.