DRV_SST39_Read Function
C
bool DRV_SST39_Read( const DRV_HANDLE handle, void *rx_data, uint32_t rx_data_length, uint32_t address )Summary
Reads n bytes of data from the specified start address of Flash memory.
Description
This function schedules a blocking operation for reading requested number of data bytes from the Flash memory.
Preconditions
The DRV_SST39_Open() routine must have been called for the specified SST39 driver instance.
Parameters
| Parameters | Description |
|---|---|
| handle | A valid open-instance handle, returned from the driver's open routine |
| rx_data | Buffer pointer into which the data read from the SST39 Flash memory will be placed |
| rx_data_length | Total number of bytes to be read |
| address | Read memory start address from where the data should be read |
Returns
True - If number of bytes requested are read from Flash memory.
False - If read command itself fails.
Example
#define BUFFER_SIZE 1024 #define MEM_ADDRESS 0x0 DRV_HANDLE handle; uint8_t CACHE_ALIGN readBuffer[BUFFER_SIZE]; if (DRV_SST39_Read(handle, (void *)&readBuffer, BUFFER_SIZE, MEM_ADDRESS) == false) { printf("Error handling here"); }
Remarks
None.