1.4.4.5 OSAL_SEM_PostISR Function
1.4.4.5 C
OSAL_RESULT OSAL_SEM_PostISR(OSAL_SEM_HANDLE_TYPE* semID)
1.4.4.5 Summary
Posts a semaphore or increments a counting semaphore from within an Interrupt Service Routine (ISR).
1.4.4.5 Description
This function posts a binary semaphore or increments a counting semaphore. The highest priority task currently blocked on the semaphore will be released and made ready to run. This form of the post function should be used inside an ISR.
1.4.4.5 Precondition
Semaphore must have been created.
1.4.4.5 Parameters
| Parameters | Description |
|---|---|
| semID | Pointer to the Semaphore ID |
1.4.4.5 Returns
OSAL_RESULT_TRUE - Semaphore posted.
OSAL_RESULT_FALSE - Semaphore not posted.
1.4.4.5 Example
void __ISR(UART_2_VECTOR) _UART2RXHandler() { char c; // read the character c = U2RXREG; // clear the interrupt flag IFS1bits.U2IF = 0; // post a semaphore indicating a character has been received OSAL_SEM_PostISR(&semSignal); }
1.4.4.5 Remarks
This version of the OSAL_SEM_Post function should be used if the program is, or may be, operating inside an ISR. The OSAL will take the necessary steps to ensure correct operation possibly disabling interrupts or entering a critical section. The exact requirements will depend upon the particular RTOS being used.