1.1.14.3.3 Configuring the Library
The W25 driver library should be configured through the MCC. The following figures show the MCC configuration window for the W25 driver and brief description.
W25 driver with QMSPI peripheral in SQI mode connected:
W25 driver with connection to Memory driver:
Configuration Options
-
PLIB Used:
-
Specifies the Peripheral library connected
-
-
W25 Protocol Used:
-
Specifies the protocol used to interface with PLIB by the W25 driver
-
-
Number of Clients:
-
Indicates maximum number of clients
-
Always set to one as it supports only a single client
-
-
W25 Start Address:
-
Specifies the Flash memory start address to be used for Transfer operations
-
The start address will be populated in the device geometry table DRV_W25_GEOMETRY
-
-
W25 Erase Buffer Size:
-
This option appears only when the W25 driver is connected to the Memory driver for block operations
-
Specifies the size for erase buffer used by Memory driver
-
The size of the buffer should be equal to erase sector size as the memory driver will call DRV_W25_SectorErase
-