7.3.1 Hardware Setup for On-Board Programming
- Mount the routing and socket card and the target device. See the Socket System section on how to do this.
- Use a 10-wire cable supplied with the STK600 to connect the PROG DATA to the target device, as shown in the picture below.
- Note that for ATtiny24/44/84, a cable on PROG CTRL is required as well, as for the Parallel High-Voltage Programming.
- Mount both the VTARGET jumper and the RESET jumper.
- Ensure that VTARGET is between 4.5 and 5.5V before programming.
See the Programming Dialog pages in the Microchip Studio help file for information on the STK600 programming dialog.