1.3.5.1.9 MAC_RF_MIB Struct
C
typedef struct
{
uint32_t retryCountRF;
uint32_t multipleRetryCountRF;
uint32_t txFailCountRF;
uint32_t txSuccessCountRF;
uint32_t fcsErrorCountRF;
uint32_t securityFailureCountRF;
uint32_t duplicateFrameCountRF;
uint32_t rxSuccessCountRF;
uint32_t nackCountRF;
uint32_t txDataPacketCountRF;
uint32_t rxDataPacketCountRF;
uint32_t txCmdPacketCountRF;
uint32_t rxCmdPacketCountRF;
uint32_t csmaFailCountRF;
uint32_t rxDataBroadcastCountRF;
uint32_t txDataBroadcastCountRF;
uint32_t badCrcCountRF;
MAC_RF_POS_TABLE_ENTRY *posTableRF;
uint16_t posTableSizeRF;
MAC_DEVICE_TABLE_ENTRY *deviceTableRF;
uint16_t deviceTableSizeRF;
MAC_RF_DSN_TABLE_ENTRY *dsnTableRF;
uint16_t dsnTableSizeRF;
uint8_t duplicateDetectionTtlRF;
uint8_t eBsnRF;
uint8_t dsnRF;
uint32_t frameCounterRF;
bool lbpFrameReceivedRF;
bool lngFrameReceivedRF;
bool bcnFrameReceivedRF;
uint32_t rxOtherDestinationCountRF;
uint32_t rxInvalidFrameLengthCountRF;
uint32_t rxWrongAddrModeCountRF;
uint32_t rxUnsupportedSecurityCountRF;
uint32_t rxWrongKeyIdCountRF;
uint32_t rxInvalidKeyCountRF;
uint32_t rxWrongFCCountRF;
uint32_t rxDecryptionErrorCountRF;
bool macSnifferRF;
uint8_t maxBeRF;
uint8_t maxCsmaBackoffsRF;
uint8_t maxFrameRetriesRF;
uint8_t minBeRF;
uint8_t operatingModeRF;
uint16_t channelNumberRF;
uint8_t dutyCycleUsageRF;
uint16_t dutyCyclePeriodRF;
uint16_t dutyCycleLimitRF;
uint8_t dutyCycleThresholdRF;
uint32_t ackTxDelayRF;
uint32_t ackRxWaitTimeRF;
uint32_t ackConfirmWaitTimeRF;
uint32_t dataConfirmWaitTimeRF;
uint16_t lastFrameDurationRF;
uint16_t posRecentEntriesRF;
bool disablePhyRF;
bool rfAvailable;
uint8_t frequencyBandRF;
uint8_t transmitAttenRF;
uint8_t adaptivePowerStepRF;
uint8_t adaptivePowerHighBoundRF;
uint8_t adaptivePowerLowBoundRF;
uint8_t beaconRandomizationWindowLength;
uint8_t trickleMinLQIRF;
} MAC_RF_MIB;Summary
Defines the MAC RF Information Base.
Description
This structure holds the MAC RF IB, it contains one field per each defined PIB.
Field description:
- retryCountRF. Statistical counter for number of transmitted packets which required one retry.
- multipleRetryCountRF. Statistical counter for number of transmitted packets which required multiple retries.
- txFailCountRF. Statistical counter for number of packets which failed in transmission.
- txSuccessCountRF. Statistical counter for number of successfully transmitted packets.
- fcsErrorCountRF. Statistical counter for number of received packets with FCS errors.
- securityFailureCountRF. Statistical counter for number of received packets with security errors.
- duplicateFrameCountRF. Statistical counter for number of duplicate received packets.
- rxSuccessCountRF. Statistical counter for number of successfully received packets.
- nackCountRF. Statistical counter for number of transmitted packets which did not received an ACK back.
- txDataPacketCountRF. Statistical counter for number of transmitted data packets.
- rxDataPacketCountRF. Statistical counter for number of received data packets.
- txCmdPacketCountRF. Statistical counter for number of transmitted command packets.
- rxCmdPacketCountRF. Statistical counter for number of received command packets.
- csmaFailCountRF. Statistical counter for number of Medium Access failures.
- rxDataBroadcastCountRF. Statistical counter for number of received broadcast packets.
- txDataBroadcastCountRF. Statistical counter for number of transmitted broadcast packets.
- badCrcCountRF. Statistical counter for number of received packets with CRC errors.
- *posTableRF. Pointer to MAC PLC POS Table.
- posTableSizeRF. Maximun number of entries in MAC PLC POS Table.
- *deviceTableRF. Pointer to MAC PLC Device Table.
- deviceTableSizeRF. Maximun number of entries in MAC PLC Device Table.
- *dsnTableRF. Pointer to MAC PLC Data Sequence Number Table.
- dsnTableSizeRF. Maximun number of entries in MAC PLC Data Sequence Number Table.
- duplicateDetectionTtlRF. Time to live for DSN Table entries.
- eBsnRF. Current Enhanced Beacon Sequence Number for transmission.
- dsnRF. Current Data Sequence Number for transmission.
- frameCounterRF. Device transmission Frame Counter.
- lbpFrameReceivedRF. Flag indicating whether Boostrap Protocol frames have been received since last read of this PIB.
- lngFrameReceivedRF. Flag indicating whether LOADng frames have been received since last read of this PIB.
- bcnFrameReceivedRF. Flag indicating whether Beacon frames have been received since last read of this PIB.
- rxOtherDestinationCountRF. Statistical counter for number of frames dropped due to different destination.
- rxInvalidFrameLengthCountRF. Statistical counter for number of frames dropped due to Invalid Length.
- rxWrongAddrModeCountRF. Statistical counter for number offrames dropped due to wrong Addressing Mode.
- rxUnsupportedSecurityCountRF. Statistical counter for number offrames dropped due to Security mismatching.
- rxWrongKeyIdCountRF. Statistical counter for number offrames dropped due to wrong Key ID.
- rxInvalidKeyCountRF. Statistical counter for number offrames dropped due to Invalid Key.
- rxWrongFCCountRF. Statistical counter for number offrames dropped due to unexpected Frame Counter.
- rxDecryptionErrorCountRF. Statistical counter for number offrames dropped due to Decryption error.
- macSnifferRF. Indicates whether MAC sniffer is active.
- maxBeRF. Maximum Backoff exponent for CSMA.
- maxCsmaBackoffsRF. Number of Backoffs for CSMA.
- maxFrameRetriesRF. Maximum retries in transmission before dropping a frame.
- minBeRF. Minimum Backoff exponent for CSMA.
- operatingModeRF. RF Operating Mode to use.
- channelNumberRF. RF Channel Number to use.
- dutyCycleUsageRF. Current Duty Cycle used in node.
- dutyCyclePeriodRF. Period to measure Duty Cycle.
- dutyCycleLimitRF. Allowed limit in Duty Cycle usage.
- dutyCycleThresholdRF. Percentage of Duty Cycle limit to stop transmitting frames (except ACKs).
- ackTxDelayRF. Time between frame reception and following ACK transmission.
- ackRxWaitTimeRF. Time to wait for ACK before retrying transmission.
- ackConfirmWaitTimeRF. Time to wait for ACK Confirm before timing out.
- dataConfirmWaitTimeRF. Time to wait for frame Confirm before timing out.
- lastFrameDurationRF. Duration, in us, of the last frame received over RF medium.
- posRecentEntriesRF. Number of POS table entries having been refreshed recently and which LQI is above adpTrickleLQIThresholdLow.
- disablePhyRF. Flag to disable RF PHY layer.
- rfAvailable. Flag to indicate whether RF interface is available.
- frequencyBandRF. RF Frequency Band to use.
- transmitAttenRF. Transmission attenuation to use for every frame, in addition to particular link configuration.
- adaptivePowerStepRF. Step (in dBm) to lowe transmission power when requested.
- adaptivePowerHighBoundRF. High limit of Tx Power hysteresis window.
- adaptivePowerLowBoundRF. Low limit of Tx Power hysteresis window.
- beaconRandomizationWindowLength. Window size to choose a random point inside to transmit a Beacon frame.
- trickleMinLQIRF. Minimum LQI to consider a neighbour for Trickle.
Remarks
None.