The TUxyCLK
            register bits select the clock source for the UTMR module. These bits allow the
            selection of several possible synchronous and asynchronous clock sources. Because the
            selected clock source also controls the optional synchronization of all external signals
            for the UTMR module, delays between the selection of a function and its action may vary
            according to the frequency of the selected clock source relative to the
            microcontroller’s clock frequency. See the Synchronous vs.
                Asynchronous Operation section for more details.
        When an internal clock source is selected (clock derived from system oscillator), the
            choice of clock source will affect the increment rate of the TUxyTMR register, relative
            to the system instruction rate. When an external clock source is selected (a clock not
            derived from the system oscillator), the UTMR module will work as either a timer or a
            counter. When enabled to count and the 
CPOL bit is set, the TUxyTMR counter register is incremented on the rising
            edge of the selected external source. For increment on the falling edge of the selected
            external clock source, the CPOL bit must be cleared. When operating from an external
            clock source, the 
CSYNC bit must also be set to synchronize the controls and ERS
            signals to the clock domain of the selected external clock. 
Important: Due to the
                inherent uncertainty of reading or writing a 
16-bit timer
                with an 8-bit bus and operating from an asynchronous clock source, it is recommended
                that read/write of the timer registers use the 
CAPT and the 
CLR commands. Refer to the 
Timer Counter and
                    Capture Registers section for more information.