1.10 PIO Interrupt
This example shows how to generate GPIO interrupt on switch press and release, and indicate the switch status using the LED.
Description
This application uses the PIO Peripheral library to generate callback on switch press and release, and drives the GPIO pin connected to the LED to indicate the switch status. The LED is turned ON when the switch is pressed and turned OFF when the switch is released.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/pio/pio_led_on_off_interrupt/firmware.
To build the application, refer to the following table and open the project using its IDE.
Project Name | Description |
---|---|
pic32cx_mtsh_db.X | MPLABX project for PIC32CXMTSH Development Board |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
Project Name | Board |
---|---|
pic32cx_mtsh_db.X | PIC32CXMTSH Development Board |
Setting Up PIC32CXMTSH Development Board
- Power on the board using a 12V power supply on J3
- Attach a debugger to the SWD/JTAG port J17
Running the Application
- Build and Program the application using its IDE
- LED is turned ON when the switch is pressed and turned OFF when the switch is
releasedFollowing table provides the Switch and LED names:
Board Switch Name LED Name PIC32CXMTSH Development Board Scroll Down D20