1.13 QSPI Flash Read Write
This example shows how to use the QSPI Peripheral library to perform erase, write and read operation with the QSPI Serial Flash memory in Quad IO mode.
Description
This example uses the QSPI peripheral library to erase and write an array of values to the QSPI Serial Flash memory. It verifies the value written by reading the values back and comparing it to the value written.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/qspi/qspi_read_write/firmware.
To build the application, refer to the following table and open the project using its IDE.
Project Name | Description |
---|---|
pic32cx_mtc_db.X | MPLABX project for PIC32CXMTC Development Board |
pic32cx_mtg_db.X | MPLABX project for PIC32CXMTG Evaluation Kit |
pic32cx_mtsh_db.X | MPLABX project for PIC32CXMTSH Development Board |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
Project Name | Board |
---|---|
pic32cx_mtc_db.X | PIC32CXMTC Development Board |
pic32cx_mtg_db.X | PIC32CXMTG Evaluation Kit |
pic32cx_mtsh_db.X | PIC32CXMTSH Development Board |
Setting Up PIC32CXMTC Development Board
- Power on the board using a 12V power supply on J3
- Attach a debugger to the SWD/JTAG port J20
Setting Up PIC32CXMTG Evaluation Kit
- Power on the board using a 5V power supply on J17
- Connect the Debug USB port on the board to the computer using a micro USB cable
Setting Up PIC32CXMTSH Development Board
- Power on the board using a 12V power supply on J3
- Attach a debugger to the SWD/JTAG port J17
Running the Application
- Build and Program the application using its IDE
- LED indicates success or failure:
- The LED is toggled when the value read from the QSPI Serial Flash memory matched with the written value
- The LED is turned ON when the value read from the QSPI Serial Flash did
not match with the written valueThe following table provides the LED name:
Board LED Name PIC32CXMTC Development Board D24 PIC32CXMTG Evaluation Kit D3 PIC32CXMTSH Development Board D20