1.3 ADC User Sequence
This example demonstrates how to sample two analog inputs using the user sequencer in software trigger mode and send the converted data to the console.
Description
Board | Sequence of Conversion |
---|---|
PIC32CXMTSH Development Board | AD1 → AD2 |
Analog input voltage in the range of 0V to 3.3V is fed to the ADC input channel AD1, AD2. ADC conversion result is displayed on the console.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/adc/adc_user_sequence/firmware.
To build the application, refer to the following table and open the project using its IDE.
Project Name | Description |
---|---|
pic32cx_mtsh_db.X | MPLABX project for PIC32CXMTSH Development Board |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
Project Name | Board |
---|---|
pic32cx_mtsh_db.X | PIC32CXMTSH Development Board |
Setting Up PIC32CXMTSH Development Board
- Use a jumper wire to connect Pin 3 of Xplained Pro Header (AD1 is mapped to Port Pin PA30) to 3.3V or GND
- Use a jumper wire to connect Pin 1 of mikroBUS Socket (AD2 is mapped to Port Pin PA31) to 3.3V or GND
- Power on the board using a 12V power supply on J3
- Attach a debugger to the SWD/JTAG port J17
Running the Application
- Open the Terminal application (Ex.: Tera term) on the computer
- Connect to the EDBG Virtual COM port and configure the serial settings as
follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
- Build and Program the application project using its IDE
- Console displays the ADC Count and the ADC Input Voltage