1.22 TC Compare Mode

This example shows how to use the TC module in compare mode to generate an active low, active high, and toggle output on compare match.

Description

Three TC channels are configured in compare mode. Each channel generates different output waveform depending upon configured action on compare match and period match.

Active low output: Output is set high on compare 1 match and is set low on compare 0 match.

Active high output: Output is set low on compare 1 match and is set high on compare 0 match.

Toggle output: Output toggles on compare 0 match.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/tc/tc_compare_mode/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project NameDescription
pic32cx_mtsh_db.XMPLABX project for PIC32CXMTSH Development Board

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project NameBoard
pic32cx_mtsh_db.XPIC32CXMTSH Development Board

Setting Up PIC32CXMTSH Development Board

  • Power on the board using a 12V power supply on J3
  • Attach a debugger to the SWD/JTAG port J17

Running the Application

  1. Build and Program the application using its IDE
  2. Observe generated waveforms on the oscilloscope
    PIC32CXMTSH Development Board:
    Timer ChannelPinObservable Characteristic of the Waveform
    TC0_TIOA1PA31 (Pin 1 of mikroBUS header)Toggle output with 50 Hz frequency
    TC0_TIOA0PA02(Pin 10 of Xplained pro header)Active high output with 100 Hz frequency
    TC0_TIOB0PA03(Pin 9 of Xplained pro header)Active low output with 100 Hz frequency