4.2.2 Atmel megaAVR with TWI Interface
The following code section contains definitions related to this target.
//******************MEGAAVR TWI PARAMETERS***********************/
#elif defined(MEGAAVR) && defined(TWI)
#include "atmega_twi_driver.h"
/*! \brief Largest message size that will be sent/received
excluding address byte and register address. When using array
write/read functions, the count parameter can not exceed
NUM_BYTES*/
#define NUM_BYTES 16
// Bit rate Register setting for 8MHz CPU clock, 100 KHz SCL
#define TWI_TWBR 0x20
#define TWI_TWPS 0x00
//*****************************************************************
- NUM_BYTES defines the maximum number of data bytes that can be sent in one transfer. It is used when using the array read/write commands. The count parameter can not exceed NUM_BYTES.
- TWI_BUFFER_SIZE defines the size of TX/RX buffer. In simple read/write transactions with MSL, three bytes are transferred one way.
- TWI_TWBR and TWI_TWPS define the baud rate register settings according to the equation below. Carefully enter these to set the SCL clock frequency.