4.2.1 Atmel XMEGA with TWI Interface
The following code section contains definitions related to this target.
//*********ATXMEGA TWI PARAMETERS******************************/
#if defined(ATXMEGA) && defined(TWI)
#include "atxmega_twi_driver.h"
/*! \brief Largest message size that will be sent/received
excluding address byte and register address. When using array
write/read functions, the count parameter can not exceed
NUM_BYTES*/
#define NUM_BYTES 16
/*! TWI port used, */
#define TWI_PORT TWIC
/*! TWI master Interrupt */
#define TWI_INT_VECTOR TWIC_TWIM_vect
/*BAUDRATE 100Khz*/
#define BAUDRATE 100000
//*****************************************************************
- NUM_BYTES defines the maximum number of data bytes that can be sent in one transfer. It is used when using the array read/write commands. The count parameter can not exceed NUM_BYTES.
- TWI_PORT defines which TWI module is used
- TWI_INIT_VECTOR defines the interrupt associated with that TWI module
- BAUDRATE defines the target SCL clock frequency in hertz. For most TWI applications, it is 100kHz.