6.2.4 Supply Controller Pinout

The outputs of the Supply Controller (SUPC) are not mapped to the normal PORT functions. They are controlled by registers in the SUPC.

Table 6-6. SUPC Pinout
SignalI/O pin
OUT0PB01
OUT1PB02
Note: If the RTC is enabled to use the pins shared with the SUPC, the RTC will have higher priority.