2.9.2 Using the Library

This topic describes the basic architecture of the USB Printer Device Library and provides information and examples on its use.

Topics

Name Description
Abstraction Model Provides an architectural overview of the Printer Function Driver.
Library OverviewThe USB Printer Device Library mainly interacts with the system, its clients and function drivers, as shown in the Abstraction Model. The library interface routines are divided into sub-sections, which address one of the blocks or the overall operation of the USB Printer Device Library.
How the Library Works This topic describes the basic architecture of the USB Printer Device Library and provides information and examples on its use.