3.4.2 Using the Library
Topics
| Name | Description | 
| Abstraction Model | Describes the Abstraction Model of the USB CDC Host Client Driver Library. | 
| Library Overview | The USB CDC Host Client Driver API is grouped functionally, as shown in the following table. | 
| How the Library Works | Describes how the Library works and how it should be used. |